SDK for LPC1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK for LPC1549

1,518 Views
DanielLongo
Contributor I

I am new to NXP MCUs and have installed MCUXpresso IDE and Config Tools. I need an SDK for the LPC1549. I am on the MCUXpresso SDK Builder page\Boards\LPC, but I don't see an option for the LPC1549. Perhaps there is a generic SDK that will work? Which one? I have the LPC1549 with JTAG and SWD connections and a dev board for the programmer/debugger. I'm just lost as to where I find the SDK to get started in MCUXpresso. Your help is very much appreciated. Thanks in advance!

Labels (1)
0 Kudos
Reply
2 Replies

1,505 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DanielLongo,

The LPC1549 is a legacy LPC from the LPCXpresso era, which is why it does not have an SDK like the newer LPC55xx or LPC8xx devices. These old LPCs used something called LPCOpen, which is a set of libraries, drivers and example codes that allow for the easy development of LPC projects (similar to SDK nowadays). You can find the LPCOpen libraries for your device on the following website: LPCOpen Libraries and Examples | NXP Semiconductors

Also, take a look at the MCUXpresso User Guide for more information on how to use LPCOpen with the IDE.

BR,
Edwin.

1,493 Views
DanielLongo
Contributor I
Thanks for the heads up. That makes sense. I'll dive into the user's guide and see if I can get it to play nice..
0 Kudos
Reply