SDK_2.3.0_LPCXpresso54608 missing RVDS folder?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK_2.3.0_LPCXpresso54608 missing RVDS folder?

1,436件の閲覧回数
johanandrade
Contributor III

Hello,

I'm trying to debug the LPCXpressro 54608 with Keil and one of the paths in the compiler settings is for "...\RVDS\ARM_CM4F". However, the SDK doesn't include the RVDS folder only the GCC. Unfortunately using the GCC files won't let me compile the program and I'm met with errors.

Image 076.png

Image 077.png

Image 078.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,329件の閲覧回数
johanandrade
Contributor III

Nevermind. Error on my part. When using the SDK builder, be sure the Keil MDK toolchain is selected and not something else. I was still using MCUXpress toolchain.

0 件の賞賛
返信