SDK_2.3.0_LPCXpresso54608 missing RVDS folder?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK_2.3.0_LPCXpresso54608 missing RVDS folder?

1,435 Views
johanandrade
Contributor III

Hello,

I'm trying to debug the LPCXpressro 54608 with Keil and one of the paths in the compiler settings is for "...\RVDS\ARM_CM4F". However, the SDK doesn't include the RVDS folder only the GCC. Unfortunately using the GCC files won't let me compile the program and I'm met with errors.

Image 076.png

Image 077.png

Image 078.png

Labels (1)
0 Kudos
Reply
1 Reply

1,328 Views
johanandrade
Contributor III

Nevermind. Error on my part. When using the SDK builder, be sure the Keil MDK toolchain is selected and not something else. I was still using MCUXpress toolchain.

0 Kudos
Reply