SD interface driver sets incorrect SD clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD interface driver sets incorrect SD clock

2,945件の閲覧回数
leecoakley
Contributor III

I was looking at the SD bus signals on a scope and I noticed the clock speeds were all WAY off the mark.

  • Set 400 KHz, get ~118 KHz.  Cards don't work. (Must be why the high level driver enumerates at 20MHz)
  • Set 20 MHz, get 16.67 MHz. Usually works but it's slower than it should be.
  • Set 50 MHz, get 33.33 MHz. Usually not tolerated.

This looks suspiciously like a divisor being stepped up one notch further than it's supposed to be.  When I went through the SDIF driver I found the culprit was exactly that.  Look at the function Chip_SDIF_SetClock(). This is how it computes the divisor:

div = ((clk_rate / speed) + 2) >> 1;

This is wrong.  It should be + 1.  Once corrected I get the expected clocks and everything works perfectly.  All cards enumerate, high speed mode works, etc.

This makes your SD controller look much worse than it actually is!  When properly configured I can run any SD card I own in high-speed mode and get the full 25 MB/sec the controller is capable of - from ancient SD to SDHC to a brand new SDXC card. The SD controller is really a great piece of work. But I can't say the same for the drivers. :smileysilly:

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,685件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Lee Coakley,

    Thanks a lot for your information sharing.

    Do you also check the clk_rate, whether it is correct on your side.

   Because, if refer to the user manual:

pastedImage_1.png

div = ((clk_rate / speed) + 2) >> 1; is correct.

clk_rate/speed= (div*2-2)=(div-1)*2

So, I think we also need to check clk_rate, whether it is correct or not.

Can you help to check these point?

     Set 400 KHz, get ~118 KHz.  Cards don't work. (Must be why the high level driver enumerates at 20MHz)

  • Set 20 MHz, get 16.67 MHz. Usually works but it's slower than it should be.
  • Set 50 MHz, get 33.33 MHz. Usually not tolerated.

Give me the above 3 situations pSDMMC->CLKDIV data with div = ((clk_rate / speed) + 2) >> 1; and div = ((clk_rate / speed) + 1) >> 1;

Please also give me the code about calling Chip_SDIF_SetClock(LPC_SDMMC_T *pSDMMC, uint32_t clk_rate, uint32_t speed), especially clk_rate and speed data.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,685件の閲覧回数
leecoakley
Contributor III

Hi Kerry, I gathered the info.

The clock is enabled in Chip_SDIF_Init():

   Chip_Clock_EnableOpts(CLK_MX_SDIO, true, true, 1);

Clk_rate is read using this function, which returns 204 MHz:

   Chip_Clock_GetBaseClocktHz(CLK_BASE_SDIO)

Used in this context:

   Chip_SDIF_SetClock(pSDMMC, Chip_Clock_GetBaseClocktHz(CLK_BASE_SDIO), g_card_info->card_info.speed);

I verified that the speed parameter makes sense. Console output:

speed = 400000
speed = 25000000
speed = 50000000

With the original computation where I observe the wrong frequency, the divisors are computed as:

  • 400 KHz: div = 256
  • 20 MHz: div = 6
  • 25 MHz: div = 5
  • 50 MHz: div = 3

With my change it's one less:

  • 400 KHz: div = 255
  • 20 MHz: div = 5
  • 25 MHz: div = 4
  • 50 MHz: div = 2

Also confirmed on the scope that these frequencies are the ones being output.

Plugging in the formula from the reference manual it looks like my formula gives the better answer:

Original:

204,000,000 / (2 * 256) =      398,438 (can't actually be set, 256 doesn't fit in the register so it was really 204MHz I guess)

204,000,000 / (2 * 6)     = 17,000,000 (15% error)

204,000,000 / (2 * 5)     = 20,400,000 (18% error)

204,000,000 / (2 * 3)     = 34,000,000 (32% error)

Revised:

204,000,000 / (2 * 255) =      400,000 (0% error)

204,000,000 / (2 * 5)     = 20,040,000 (2% error)

204,000,000 / (2 * 4)     = 25,500,000 (2% error)

204,000,000 / (2 * 2)     = 51,000,000 (2% error)

Adding + 1 picks the nearest divisor resulting in the best match, adding + 2 rounds up the divisor which overshoots the division rate in all cases other than exact multiples.

Here's a plot in 100KHz increments with blue as the target and red as the actual output:

divisor plot.png

Swept over the range, the average error is halved in the revised version.

0 件の賞賛
返信