SD card with LPC55s69-EVK - Peripherals Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD card with LPC55s69-EVK - Peripherals Tool

1,642 Views
BabyBorisova
Contributor II

Hey, 

I'm working with the LCP5569-EVK and wish to add an SD card as external memory.
I've looked through the demo code and it seems pretty straight forward.
I was wondering if its possible to set up the SD in MCUexpressos peripherals tool as I've done with SPI etc.

Kind regards, 
Lexi

Labels (1)
0 Kudos
Reply
1 Reply

1,637 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  BabyBorisova,

There is SD card demo under SDK, you can have a look, download from:

https://mcuxpresso.nxp.com/en/select

 

BR

Alice

0 Kudos
Reply