SD card with LPC55s69-EVK - Peripherals Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD card with LPC55s69-EVK - Peripherals Tool

1,664件の閲覧回数
BabyBorisova
Contributor II

Hey, 

I'm working with the LCP5569-EVK and wish to add an SD card as external memory.
I've looked through the demo code and it seems pretty straight forward.
I was wondering if its possible to set up the SD in MCUexpressos peripherals tool as I've done with SPI etc.

Kind regards, 
Lexi

ラベル(1)
0 件の賞賛
返信
1 返信

1,659件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  BabyBorisova,

There is SD card demo under SDK, you can have a look, download from:

https://mcuxpresso.nxp.com/en/select

 

BR

Alice

0 件の賞賛
返信