SAMPLE GUI PROJECT FOR LPC1788 WITH RGB (TFT) LCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SAMPLE GUI PROJECT FOR LPC1788 WITH RGB (TFT) LCD

1,610 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shivaraj on Tue Sep 24 04:58:01 MST 2013
Hi,

I'm new to lpc1788. I want to create a project with sample GUI.
I'm using 4.3" LCD which is directly connected to LPC1788 controller( RGB mode ).
I tried to implement basic GUI using emwin 5.22. Got negetive result.
If any one have the sample project for customized lpc1788 board, Please share it with me.

Thanks in advance,
Shivaraj HK
标签 (1)
0 项奖励
回复
2 回复数

1,452 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shivaraj on Wed Sep 25 01:58:09 MST 2013
Hi MC,

I have integrated GUI ( which you ve given in the link )into my project successfully.

Thanks a lot for your help  :)
0 项奖励
回复

1,452 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Sep 24 05:51:25 MST 2013
Hi Shivraj,
Did you try BSP that is done for the Embedded Artists EA1788 board? You can customize it according to your need.
Please see below link

http://www.lpcware.com/content/nxpfile/emwin-522-board-support-package-ea1788-board
0 项奖励
回复