SAMPLE GUI PROJECT FOR LPC1788 WITH RGB (TFT) LCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAMPLE GUI PROJECT FOR LPC1788 WITH RGB (TFT) LCD

1,688 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shivaraj on Tue Sep 24 04:58:01 MST 2013
Hi,

I'm new to lpc1788. I want to create a project with sample GUI.
I'm using 4.3" LCD which is directly connected to LPC1788 controller( RGB mode ).
I tried to implement basic GUI using emwin 5.22. Got negetive result.
If any one have the sample project for customized lpc1788 board, Please share it with me.

Thanks in advance,
Shivaraj HK
Labels (1)
0 Kudos
Reply
2 Replies

1,530 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shivaraj on Wed Sep 25 01:58:09 MST 2013
Hi MC,

I have integrated GUI ( which you ve given in the link )into my project successfully.

Thanks a lot for your help  :)
0 Kudos
Reply

1,530 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Sep 24 05:51:25 MST 2013
Hi Shivraj,
Did you try BSP that is done for the Embedded Artists EA1788 board? You can customize it according to your need.
Please see below link

http://www.lpcware.com/content/nxpfile/emwin-522-board-support-package-ea1788-board
0 Kudos
Reply