Reset and Watchdog IC to be used along with LPC4367

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset and Watchdog IC to be used along with LPC4367

1,512 Views
manish_sharma2
Contributor II

Hi,

I am using LPC4367JBD208E in my product. I Need to know the Reset and Watchdog IC to be used along with LPC4367 to reset it.

 

Thanks

Manish Sharma

0 Kudos
Reply
4 Replies

1,467 Views
frank_m
Senior Contributor III

Read the datasheet and user manual of your MCU.

0 Kudos
Reply

1,491 Views
manish_sharma2
Contributor II

Dear Sir,

Hi, Xiang

Kindly let me know what is the RESET pin current required to reset the LPC4367 MCU.
It is not clearly mentioned in the datasheet.

Thanks
Manish

0 Kudos
Reply

1,479 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport
Hi, The Reset pin is a general standard input pin, the leakage current is about 3nA typically in both high or low logic input. Pls download the data sheet of LPC436x from the following link and refer to section Table 11. Static characteristics …continued, check the Ill and Ilh specs. https://www.nxp.com.cn/docs/en/data-sheet/LPC436X.pdf Hope it can help you Regard XiangJun Rong
0 Kudos
Reply

1,506 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Manish,

The LPC4367 has internal power-On Reset and watch dog, so in general, it is okay to use an RC circuit for the Reset pin, external watch dog is not required.

If you do want to use external Reset circuit, I do not think there is special requirement for the Reset circuit, anyway, you can consider UM805/UM811/UM812.

Regarding the external watch dog, I have not idea. But you can search it on Google.

BR

XiangJun rong

0 Kudos
Reply