Register values in UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Register values in UART

1,845 Views
rudomanenko
Contributor II

Hi! I am using LPC11uxx and trying to configurate UART smart card mode. When I filled register DLM value, IER also fiiled by the same value? Is it normal? If yes, why it is happens? 

Labels (1)
2 Replies

1,686 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Anton Rudomanenko,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) When I filled register DLM value, IER also filled by the same value?
-- Yes, their address is identical, however, the value of DLAB bit determine the writing value be valid or not.

pastedImage_1.png
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,686 Views
rudomanenko
Contributor II

thanks a lot, jeremyzhou, but I can't show you code and hardware - it's private project

0 Kudos
Reply