Regading MP3 streamer for LPC4333

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regading MP3 streamer for LPC4333

1,118 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shilpa on Wed Mar 20 04:59:16 MST 2013
Is any MP3 streamer available for LPC4333(512 KB of flash)? The operating system we are planning to use is FreeRTOS and the IP stack is LWIP.



Labels (1)
0 Kudos
Reply
1 Reply

1,107 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Mon Apr 01 10:44:19 MST 2013
Embedded Artists has a nice MP3 demo for their EA-LPC4088 development board. It is easily portable to the Keil MCB4300 board.

NXP is currently working on a LAN radio demo that uses LWIP and FreeRTOS for the Keil MCB4300 board. It will become available in a month or so and will also show up as an example on a future release of LPCOpen Platform.
0 Kudos
Reply