Regading MP3 streamer for LPC4333

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regading MP3 streamer for LPC4333

1,126件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shilpa on Wed Mar 20 04:59:16 MST 2013
Is any MP3 streamer available for LPC4333(512 KB of flash)? The operating system we are planning to use is FreeRTOS and the IP stack is LWIP.



ラベル(1)
0 件の賞賛
返信
1 返信

1,115件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Mon Apr 01 10:44:19 MST 2013
Embedded Artists has a nice MP3 demo for their EA-LPC4088 development board. It is easily portable to the Keil MCB4300 board.

NXP is currently working on a LAN radio demo that uses LWIP and FreeRTOS for the Keil MCB4300 board. It will become available in a month or so and will also show up as an example on a future release of LPCOpen Platform.
0 件の賞賛
返信