Reference Ethernet clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reference Ethernet clock

1,353 次查看
AFZ
Contributor I

Hi,

i am using LPC2388FBD144,551 mcu.

The pin NO 126 of mcu  "ENET_REF_CLK" is being used for ethernet clock reference.

i am using 50MHz oscillator for ethernet clock and on the other side i am connecting same oscillator PAD to pin 126 of mcu.

due to mechnical reasons and board component density i cannot place mcu and ethernet block close to each other.  oscillator 50 MHz is near to ethernet block but the trace length of 50MHz reference clock connecting to mcu is very long. > 50mm

can you please suggest some solution ?

Thanks

Regards

AH

0 项奖励
回复
1 回复

1,345 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Afzal,

The trace length of 50MHz Enet_REF_CLK signal is greater than 5CM, if you use a 4 layer board(top/bottom are signal layers, the VDD/GND are power layers), i think it is okay. If you develop two layers board, I suggest you paste copper on the opposite side of the Enet_REF_CLK signal.

Anyway, 4 layer board is recommended.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复