Reference Ethernet clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reference Ethernet clock

1,311件の閲覧回数
AFZ
Contributor I

Hi,

i am using LPC2388FBD144,551 mcu.

The pin NO 126 of mcu  "ENET_REF_CLK" is being used for ethernet clock reference.

i am using 50MHz oscillator for ethernet clock and on the other side i am connecting same oscillator PAD to pin 126 of mcu.

due to mechnical reasons and board component density i cannot place mcu and ethernet block close to each other.  oscillator 50 MHz is near to ethernet block but the trace length of 50MHz reference clock connecting to mcu is very long. > 50mm

can you please suggest some solution ?

Thanks

Regards

AH

0 件の賞賛
返信
1 返信

1,303件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Afzal,

The trace length of 50MHz Enet_REF_CLK signal is greater than 5CM, if you use a 4 layer board(top/bottom are signal layers, the VDD/GND are power layers), i think it is okay. If you develop two layers board, I suggest you paste copper on the opposite side of the Enet_REF_CLK signal.

Anyway, 4 layer board is recommended.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信