Reduce Power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reduce Power consumption

1,609件の閲覧回数
jigar1
Contributor I

I am using lpc84x max board. Currently without any power down mode, my current consumption is 30mA. I want to reduce it to below 10mA. What is the best suitable option for me?

I am hardly using 6 GPIOs. I am not using SPI, I2C or other special functions. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,543件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

I suggest you try Sleep mode or Deep sleep mode.

According to datasheet, in an ideal testing environment,  for Sleep mode

pastedImage_2.png

If in your actual condition, you can't keep current consumption below 10mA with Sleep mode, Deep sleep mode should work for you.

For more information, please check LPC84x datasheet.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信