Reagarding canopen error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reagarding canopen error

1,390件の閲覧回数
saluguvenkat
Contributor I
I am getting this error message when I sent the below message,
COBID: 601h
Message sent: 2B 60 60 00 01   (I am changing the operation mode to PP)
Error msg: 80 60 60 00 12 00 07 06
Please explain the message structure if any body has the knowledge on it.
Error code:
Error register:
and rest of the field.
0 件の賞賛
返信
1 返信

1,339件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi venakat salugu
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to refer to this web page:
http://www.byteme.org.uk/?s=SDO
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信