Reagarding canopen error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reagarding canopen error

1,374 次查看
saluguvenkat
Contributor I
I am getting this error message when I sent the below message,
COBID: 601h
Message sent: 2B 60 60 00 01   (I am changing the operation mode to PP)
Error msg: 80 60 60 00 12 00 07 06
Please explain the message structure if any body has the knowledge on it.
Error code:
Error register:
and rest of the field.
0 项奖励
回复
1 回复

1,323 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi venakat salugu
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to refer to this web page:
http://www.byteme.org.uk/?s=SDO
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复