Random ADC failure in burst MODE on LPC1769 - OM13000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Random ADC failure in burst MODE on LPC1769 - OM13000

1,000 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by afinezzo1968 on Mon Aug 25 08:10:10 MST 2014
Debugging the API function which reads the 6 allowable ADC pins, the DC voltage on 6 trimmers, and write them on 3 output channels, it seems that the ADC returns some peaks not reasonable admitted, considering the environmental electric noise.

Neither connecting the AD0.x pins  to 6 bigger ceramic capacitors nor reducing the ADC clock speed by the CLKDIV bits the problem have been fixed.

The issue have been fixed by implementing a specialized function which removes the wrong values, stored in a big buffer, prior their usage.

The ADC is initialized to work in BURST mode (no interrupt and no DMA), so a function in the main loop calls periodically the readings of the 6 result registers when all the 6 DONE flags  are ready.

Somebody know how it could be fixed in a different way, or explaining the cause?

Thanks in advance
标签 (1)
0 项奖励
回复
0 回复数