RTC input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC input

2,349件の閲覧回数
Leon797
Contributor I

Is it possible to insert LVCMO signal into the RTC input?

0 件の賞賛
返信
4 返答(返信)

2,337件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Leon,

I  never hear about the "LVCMO" signal, can you tell us the part number you are using? where the "LVCMO" signal is?

BR

XiangJun Rong

0 件の賞賛
返信

2,331件の閲覧回数
Leon797
Contributor I

I meant LVCMOS

0 件の賞賛
返信

2,322件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you can see in the following Fig, the RTCXIN/RTCXOUT pins can only connect to Crystal, it can not connect to clock source which outputs squarewave clock signal directly.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1608008841021.png

 

0 件の賞賛
返信

2,318件の閲覧回数
Leon797
Contributor I

Thank you for your response

0 件の賞賛
返信