RTC clock get time and date from LPC54618

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC clock get time and date from LPC54618

ソリューションへジャンプ
3,463件の閲覧回数
gmk1
Contributor III

I'm trying to use the internal RTC clock module as per configuration below. Initialization seems okay. 

But variable "date" does not increment seconds and so is the variable "mydate".

What could be wrong?

Here is my RTC config - 

rtc_datetime_t date;

rtc_datetime_t mydate;

In Main

{

   RTC_Config();

   while(1)

   {

      RTC_GetDatetime(RTC,&date);      // seconds should be incrementing at 1 sec rate but it doesn't

      mydate = date;

   }

}

void RTC_Config(void)
{

/* Enable the external RTC 32K Oscillator */
SYSCON->RTCOSCCTRL |= SYSCON_RTCOSCCTRL_EN_MASK;
/* Init RTC */
RTC_Init(RTC);
/* Set a start date & time */
date.year = 2019U;
date.month = 2U;
date.day = 9U;
date.hour = 9U;
date.minute = 0;
date.second = 0;
/* RTC time counter has to be stopped before setting the date & time in the TSR register */
RTC_StopTimer(RTC);
/* Set RTC time to default */
RTC_SetDatetime(RTC, &date);
/* Start the RTC time counter */
RTC_StartTimer(RTC);
}

-Gmk

ラベル(4)
1 解決策
3,177件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I don't have exact your board, but I just tested your issue with my LPC54608 board.

I use mcuxpresso demo code under  ..\LPC54608\SDK_2.5.0_LPCXpresso54608\boards\lpcxpresso54608\driver_examples\rtc

I commented

   // RTC_EnableInterrupts(RTC, kRTC_AlarmInterruptEnable);

   // EnableIRQ(RTC_IRQn);

Thus my code should be same as yours.

when I step over code, I can see RTC->COUNT value changed after "RTC_StartTimer()". So I can't reproduce your issue.

I would suggest you test the same demo code on your side, comparing the register setting of the demo with your working project to shoot trouble.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

6 返答(返信)
3,178件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I don't have exact your board, but I just tested your issue with my LPC54608 board.

I use mcuxpresso demo code under  ..\LPC54608\SDK_2.5.0_LPCXpresso54608\boards\lpcxpresso54608\driver_examples\rtc

I commented

   // RTC_EnableInterrupts(RTC, kRTC_AlarmInterruptEnable);

   // EnableIRQ(RTC_IRQn);

Thus my code should be same as yours.

when I step over code, I can see RTC->COUNT value changed after "RTC_StartTimer()". So I can't reproduce your issue.

I would suggest you test the same demo code on your side, comparing the register setting of the demo with your working project to shoot trouble.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,177件の閲覧回数
gmk1
Contributor III

Actually I forgot to mount capacitors near crystal section and thus not providing ground to it.

Now its working. I've already replied myself to the question about this and it is under moderation when I'm writing this. 

Thanks anyway.

0 件の賞賛
返信
3,177件の閲覧回数
gmk1
Contributor III

No worries. Its working. My mistake. I forgot to mount capacitors between crystal and ground.

0 件の賞賛
返信
3,177件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

That's ok. Thanks for your sharing. :-)

0 件の賞賛
返信
3,177件の閲覧回数
gmk1
Contributor III

Hi ZhangJennie,

Can you help me with this one - https://community.nxp.com/thread/496377 

0 件の賞賛
返信
3,177件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Manikata,

I checked internally that my colleague has taken your CAN transmission thread and is working on it. Don't worry.

Have a nice day,

Jennie Zhang

0 件の賞賛
返信