RTC calibration in LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC calibration in LPC55S69

ソリューションへジャンプ
1,629件の閲覧回数
gnichimohamed
Contributor III

Hello,

In the LPC55S69 there is no mentioning of RTC calibration, do you have any idea how we can do it?

Thanks for the help!

0 件の賞賛
返信
1 解決策
1,621件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello gnichimohamed,

 

Sorry LPC55s69 doesn't support RTC calibration. 

32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power
domain. A timer in the RTC can be used for wake-up from all low power modes
including deep power-down, with 1 ms resolution. The RTC is clocked by the
32 kHz FRO or 32.768 kHz external crystal.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,622件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello gnichimohamed,

 

Sorry LPC55s69 doesn't support RTC calibration. 

32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power
domain. A timer in the RTC can be used for wake-up from all low power modes
including deep power-down, with 1 ms resolution. The RTC is clocked by the
32 kHz FRO or 32.768 kHz external crystal.

 

BR

Alice

0 件の賞賛
返信