RTC calibration in LPC55S69

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC calibration in LPC55S69

Jump to solution
1,645 Views
gnichimohamed
Contributor III

Hello,

In the LPC55S69 there is no mentioning of RTC calibration, do you have any idea how we can do it?

Thanks for the help!

0 Kudos
Reply
1 Solution
1,637 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello gnichimohamed,

 

Sorry LPC55s69 doesn't support RTC calibration. 

32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power
domain. A timer in the RTC can be used for wake-up from all low power modes
including deep power-down, with 1 ms resolution. The RTC is clocked by the
32 kHz FRO or 32.768 kHz external crystal.

 

BR

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,638 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello gnichimohamed,

 

Sorry LPC55s69 doesn't support RTC calibration. 

32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power
domain. A timer in the RTC can be used for wake-up from all low power modes
including deep power-down, with 1 ms resolution. The RTC is clocked by the
32 kHz FRO or 32.768 kHz external crystal.

 

BR

Alice

0 Kudos
Reply