REset pin required by LPC-LINK debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

REset pin required by LPC-LINK debugger

846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Wed Nov 27 17:57:36 MST 2013
Greetings,

I have always used 3 signals to the debugger header on my lpc111x designs so far: SWDIO, SWCLK & RESET. However I recently noticed that the LPC-LINK never pulls RESET low. So could I just leave RESET off the connector entirely? The reason I ask is that we are looking at the LPC8xx series with just 20 pins and being able to lose only 2 pins for debugging rather than 3 is a real plus.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)