Questions re USB device using ROM functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Questions re USB device using ROM functions

1,175 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by g40 on Thu Jan 21 04:43:48 MST 2016
Hi, can anyone help with the following?

I've got a working bulk mode loopback test that more or less works as expected with an NXP Xpresso 4337 board connected to a Windows 7 host. EP0 custom (vendor) requests also work.

1. What's the state re thread-safety for the ROM functions? If I add a systick handler and enable the ticker then USB dies.

2. Does anyone have a working isochronous example? Or even some documentation? Simply changing the relevant descriptors entries does not work

3. Is there any progress on source code and/or debug support for the ROM functions? I really don't understand why this is closed-source ...

TAIA

Jerry.

标签 (1)
0 项奖励
回复
1 回复

1,158 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by g40 on Thu Jan 28 06:48:51 MST 2016
Can anyone help with these questions? Thanks.
0 项奖励
回复