Questions re USB device using ROM functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions re USB device using ROM functions

1,232 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by g40 on Thu Jan 21 04:43:48 MST 2016
Hi, can anyone help with the following?

I've got a working bulk mode loopback test that more or less works as expected with an NXP Xpresso 4337 board connected to a Windows 7 host. EP0 custom (vendor) requests also work.

1. What's the state re thread-safety for the ROM functions? If I add a systick handler and enable the ticker then USB dies.

2. Does anyone have a working isochronous example? Or even some documentation? Simply changing the relevant descriptors entries does not work

3. Is there any progress on source code and/or debug support for the ROM functions? I really don't understand why this is closed-source ...

TAIA

Jerry.

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by g40 on Thu Jan 28 06:48:51 MST 2016
Can anyone help with these questions? Thanks.
0 Kudos
Reply