Question, LPC183x reference board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, LPC183x reference board

2,164 Views
SLICE
Contributor IV

Dear team,

My customer is investigating if they can use NXP/LPC183x for their products.

They want to use its two USB ports as High Speed.

And they want to obtain EVB or its schematic which LPC183x is used with TWO USB High Speed as reference.

They already found your LPC1837 Xplorer board can support one USB High Speed and one USB Full Speed. But they want to use two USB High Speed ports.

Do you know what board supports two USB high speed ports?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
4 Replies

1,971 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Masamichi Miyamoto,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Unfortunately, there are no boards that support two USB High Speed port.
Hope this is clear.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,971 Views
SLICE
Contributor IV

Hi jeremyzhou

Thanks for your support.

Any reference designs? No need to be checked for its actual behaviour.

Best Regards,

Miyamoto

0 Kudos
Reply

1,971 Views
SLICE
Contributor IV

Hello jeremyzhou

I found the AN11309 application note which describes about high-speed USB.

Is it helpful for using two high-speed USBs?

BR,

Miyamoto

0 Kudos
Reply

1,971 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Masamichi Miyamoto,

Thanks for your reply.

1) Is it helpful for using two high-speed USBs?

-- Yes, it's very helpful.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply