Programmability of LPC2142FBD64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Programmability of LPC2142FBD64

2,403 次查看
arsaenz
Contributor I

Hello,

Can someone confirm if the LPC2142FBD64.151 is fully programmable (outside of trimming) at the customer level? Or is it programmed at final test prior to shipment? Thank you.


Regards,

Alex

标签 (1)
0 项奖励
回复
2 回复数

2,195 次查看
Watonrin
Contributor I

I need the lpc2142 crown xti2000 hex file

0 项奖励
回复

2,295 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @arsaenz 

 

"

1. if customer do not ask NXP or 3rd party programmed the chip, the LPC2142 should be fully programmable when customer received the chip.

2. if customer asked 3rd party programmed the chip with dedicate binary, the DISTY support the program service according to the agreement with end customer, if the LPC2142 programmed by DISTY, the silicon maybe blocked by CRP(Code Read Protection), then the LPC2142 can be programmed or not is depends on the CRP set level. Please contact the service vendor.

"

BR

Alice

0 项奖励
回复