Programmability of LPC2142FBD64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programmability of LPC2142FBD64

2,451件の閲覧回数
arsaenz
Contributor I

Hello,

Can someone confirm if the LPC2142FBD64.151 is fully programmable (outside of trimming) at the customer level? Or is it programmed at final test prior to shipment? Thank you.


Regards,

Alex

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,243件の閲覧回数
Watonrin
Contributor I

I need the lpc2142 crown xti2000 hex file

0 件の賞賛
返信

2,343件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @arsaenz 

 

"

1. if customer do not ask NXP or 3rd party programmed the chip, the LPC2142 should be fully programmable when customer received the chip.

2. if customer asked 3rd party programmed the chip with dedicate binary, the DISTY support the program service according to the agreement with end customer, if the LPC2142 programmed by DISTY, the silicon maybe blocked by CRP(Code Read Protection), then the LPC2142 can be programmed or not is depends on the CRP set level. Please contact the service vendor.

"

BR

Alice

0 件の賞賛
返信