Problems migrating from 5.24 to 5.30

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems migrating from 5.24 to 5.30

1,089件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Tue Apr 26 01:13:00 MST 2016
I cross-post here too (my original post on Segger's forums).

I'm using pre-compiled emWin libraries from NXP. In my project, I was using emWin version 5.24 and now I'd like to upgrade to the latest version distributed from NXP that is 5.30c.

I have some problems with new version. The project is compiled in LPCXpresso and runs in LPC1778 MCU. The touchscreen display is based on ILI9341 controller connected to the MCU through a 16-bits parallel bus.

It seems the new version redraws some parts of the screen, even if it isn't necessary. This produces a bad flicker effect.

For example, I have a screen with 5 horizontal buttons. When I touch a button, it changes its background color, so the touched button is redrawn... and this is ok. However all the other buttons are redrawn at the same time, even if they appearence don't change.

Why this bad behaviour? If you want, I can create a test application that shows this.
ラベル(1)
0 件の賞賛
返信
1 返信

1,008件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信