Problems in reading SST26VF032 FLash via SPIFI intercace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems in reading SST26VF032 FLash via SPIFI intercace

1,663件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ashgupta28 on Wed Jan 28 03:06:24 MST 2015
[color=#036]Hello,

I am trying to use SPIFI interface LPC18xx with SST26VF032 Quad Flash chip.

I have added the public function "SPIFI_DEV_FAMILY_T *SPIFI_REG_FAMILY_SST_2Byte_PStatus(void) " in file spifilib_fam_spa_2b_pstat.c
{
static SPIFI_DEV_FAMILY_T handle;
static SPIFI_FAM_DESC_T desc;

/* Store the device specific info so it can be returned */
desc.pFamName = "Micrchip SST26VF032 based family";
desc.pDevList = &devHead;
desc.prvDataSize = PRVDATASIZE;
desc.pPrvDevGetID = deviceGetID;
desc.pPrvDevSetup = devSetup;
desc.pPrvDevRegister = devRegister;

/* Save the descriptor in the handle */
handle.pDesc = &desc;

/* Make sure that the base list is empty and the count reflects 0 */
devHead.pNext = NULL;
devCount = 0;

{

static const SPIFI_DEV_PDATA_T pData = {
            "SST26VF032",
{{0xBF, 0x26, 0x02}, 0, {0}},/* JEDEC ID, extCount, ext data  */
64,/* # of blocks */
0x10000,/* block size */
0,    /* # of sub-blocks  32 (This device only has sub-block erase in first/last 2 blocks) */
0,    /* sub-block size  0x1000 */
0x100,/* page size */
32768,/* max single read bytes */
40000000,/* max clock rate in Hz */
(SPIFI_CAP_QUAD |  SPIFI_CAP_NOBLOCK)/* capabilitites */
};
static SPIFI_DEV_DATA_T data;

data.pDevData = &pData;
devRegister(&handle, &data);
}



/* finally return the handle */
return &handle;
}


I AM SUCCESSFULLY READING JDEC ID from the function "static void deviceGetID(uint32_t spifiAddr, SPIFI_DEVICE_ID_T *pID)"
BUT OTHER THAN THAT ALL THE REGISTERS(STATUS REGISTERS, SEC ID), I AM ALWAYS GETTING 0xFF values. I guess my set up is correct as i am able to read JDEC ID
with the following function
static void deviceGetID(uint32_t spifiAddr, SPIFI_DEVICE_ID_T *pID)
{
uint8_t idx;
LPC_SPIFI_CHIPHW_T *pSpifiCtrlAddr = (LPC_SPIFI_CHIPHW_T *) spifiAddr;

/* Read ID command, plus read 3 bytes on data */
spifi_HW_SetCmd(pSpifiCtrlAddr,
(SPIFI_CMD_OPCODE(CMD_RDID) |
SPIFI_CMD_DATALEN(3 + pID->extCount) |
SPIFI_CMD_FIELDFORM(SPIFI_FIELDFORM_ALL_SERIAL) |
SPIFI_CMD_FRAMEFORM(SPIFI_FRAMEFORM_OP)));

/* Get info from the device */
pID->mfgId[0] = spifi_HW_GetData8(pSpifiCtrlAddr);/* Manufacturers ID */
pID->mfgId[1] = spifi_HW_GetData8(pSpifiCtrlAddr);/* Memory Type */
pID->mfgId[2] = spifi_HW_GetData8(pSpifiCtrlAddr);/* Memmory Capacity */

DEBUGOUT("DEVICE ID:  0x%x   0x%x   0x%x\n", pID->mfgId[0],pID->mfgId[1],pID->mfgId[2]);
/* Read the specified number of extended bytes */
for (idx = 0; idx < pID->extCount; ++idx) {
pID->extId[idx] = spifi_HW_GetData8(pSpifiCtrlAddr);
}

spifi_HW_WaitCMD(pSpifiCtrlAddr);
}

HERE I AM GETTING CORRECT VALUES 0xBF,  0x26, 0x02 BUT in this function while reading status register with command 0x05 :- I AM GETTING 0xFF values
static uint8_t prvGetStatusRegister(LPC_SPIFI_CHIPHW_T *pSpifiCtrlAddr)
{
uint8_t statRegister;

spifi_HW_SetCmd(pSpifiCtrlAddr,
(SPIFI_CMD_OPCODE(CMD_RDSR) |
SPIFI_CMD_DATALEN(1) |
SPIFI_CMD_FIELDFORM(SPIFI_FIELDFORM_ALL_SERIAL) |
SPIFI_CMD_FRAMEFORM(SPIFI_FRAMEFORM_OP)));

statRegister = spifi_HW_GetData8(pSpifiCtrlAddr);
DEBUGOUT("READ Status RAW DATA:  0x%x\n", statRegister);
/* Wait for command to complete */
spifi_HW_WaitCMD(pSpifiCtrlAddr);

return 0;
}



PLEASE HELP

THANKS,
Ashish Gupta[/color]
ラベル(1)
0 件の賞賛
返信
1 返信

1,404件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Jan 28 13:05:00 MST 2015
Hi Ahish,
Could you please get the latest library from
http://www.lpcware.com/SPIFI

and add your changes. I think it will be easier to support with latest version of lib.
0 件の賞賛
返信