Problems With DMA while receiving Video data at 27 MHz Data Rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems With DMA while receiving Video data at 27 MHz Data Rate

1,183 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chidambaramnkl on Thu Mar 31 11:03:07 MST 2016
we used SCT Module and DMA to capture video data. DMA is Triggered every Pixel clock (27MHz) to read video data at port 4 and store it in SD RAM.we made the DMA Configuration similar to application initialization note(AN11365v1.2).Problem is that DMA transfers half of the horizontal line data i.e. 720 bytes instead of 1440 bytes.We are running the application using  lpc link 2 debugger.Micro Controller running at 204 MHz Speed. Will running by  debugger  affects the performance of the DMA. Please help to solve the problem.
Labels (1)
0 Kudos
Reply
1 Reply

1,167 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply