lpc4330 MII Interface TFBGA180, pin missing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc4330 MII Interface TFBGA180, pin missing?

1,440 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ljminti on Thu Mar 31 06:17:04 MST 2016
Hi,

during reading the LPC43xx Datasheet, i'm a little confused about the MII Interface.
If i'm right, the LPC4330FET180 has an MII-Interface. However the ENET_RX_CLK as well as the ENET_TX_ER Signal that is used for the external PHY is only avalable in the BGA256 package.

The question is now, how to connect the BGA180 version with MII-Interface to an external PHY?

Julien
Labels (1)
0 Kudos
Reply
3 Replies

1,422 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,422 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ljminti on Thu Mar 31 23:55:40 MST 2016
Well,
in the Datasheet (page 819) it is written:

Quote:
The MII is not available on the LQFP144 and TFBGA100 packages.

.

For me the package TFBGA180 is ready for MII.

0 Kudos
Reply

1,422 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Mar 31 20:23:10 MST 2016
Perhaps you have to use RMII on that package.
Mike.
0 Kudos
Reply