Problem with USB Mass Storage Device when executing from SPIFI on LPC1850

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with USB Mass Storage Device when executing from SPIFI on LPC1850

1,331 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by j.daheron on Fri Jul 27 01:11:00 MST 2012
Hi,

I'm developing a Mass Storage Device application using nxpUSBlib v0.95 running on LPC1850 (Keil MCB1800 Dev. Board).
I work on example code provided with the library, but I've changed the virtual disk to be in RAM area (some kB only).
The application works fine when running from RAM (like in the example), but the device is not recognized when the application runs from SPIFI.

Could someone help me to understand why ?

Thanks,

--
Julien
标签 (1)
0 项奖励
回复
0 回复数