Problem with USB Mass Storage Device when executing from SPIFI on LPC1850

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with USB Mass Storage Device when executing from SPIFI on LPC1850

1,309 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by j.daheron on Fri Jul 27 01:11:00 MST 2012
Hi,

I'm developing a Mass Storage Device application using nxpUSBlib v0.95 running on LPC1850 (Keil MCB1800 Dev. Board).
I work on example code provided with the library, but I've changed the virtual disk to be in RAM area (some kB only).
The application works fine when running from RAM (like in the example), but the device is not recognized when the application runs from SPIFI.

Could someone help me to understand why ?

Thanks,

--
Julien
Labels (1)
0 Kudos
Reply
0 Replies