Problem with LPC51U68 by SWD ST-Link(v2) in IAR.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with LPC51U68 by SWD ST-Link(v2) in IAR.

2,347件の閲覧回数
trumozhay
Contributor I

In: I have problem with SWD ST-Link(v2) in IAR(7.30, 7.50, 8.20/8.30). Connected by 3 wire (GND, SWDIO, SWCLK). Production prototype board on LPC51U68. Flashed by USB in mass-storage mod (cool!).

Have: When try to debug or flash CPU write log "No reset"(or kind a) and "unable to read CPU-ID from Cortex CPU". Oscill show that on both SWD line presents activity. Same debugger work OK with STM32(and other) under IAR .

Q1: I need to modify my ST-Link to get right #RESET to reset board?

Q2: Anybody debug this CPU by ST-Link (and his clone) under IAR? What option I need to set for correct work?

(Sorry for ugly language...)

ラベル(1)
0 件の賞賛
返信
1 返信

2,238件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

Unfortunately, because the ST-LinkV2 is made for ST products, I do not have a way to test this with you. In addition I do not have information on the modifications that you may need to make to work with the LPC.

What I am able to do is check your schematic for the debug portion to see if there is anything wrong. If you could please send me that portion of your schematic I would be happy to review it. 

As far as the debugger, I would recommend to check the following posts as there may be some additional aspects you may need to consider to use the ST-LinkV2 with the LPC.

LPC13xx/LPC17xx with ST-Link

Using ST-Link to debug LPC1700 MCU

Have a great day!

Sabina

0 件の賞賛
返信