Problem with LPC4330-Xplorer and LPC-Link(HID)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with LPC4330-Xplorer and LPC-Link(HID)

683件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Willi.L on Fri Jun 28 05:59:45 MST 2013

I have a follow problem:


I use LPCExpresso (v5.2.4) and LPCXplorer4330.


If I debug the LPC4330-Xplorer_LedToggle-Example (without changes) with LPC-Link2 (Debugger set to RedProbe), it works fine.


If I debug the same axf.-file with LPC-Link (Debugger set to LPC-Link(HID)), it works not correct. I can debug, but the processor stays in systick_delay(),


because the SysTick_Handler(void) will not be run.


Have anyone idee, what is the cause?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)