Problem with LPC4330-Xplorer and LPC-Link(HID)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with LPC4330-Xplorer and LPC-Link(HID)

673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Willi.L on Fri Jun 28 05:59:45 MST 2013

I have a follow problem:


I use LPCExpresso (v5.2.4) and LPCXplorer4330.


If I debug the LPC4330-Xplorer_LedToggle-Example (without changes) with LPC-Link2 (Debugger set to RedProbe), it works fine.


If I debug the same axf.-file with LPC-Link (Debugger set to LPC-Link(HID)), it works not correct. I can debug, but the processor stays in systick_delay(),


because the SysTick_Handler(void) will not be run.


Have anyone idee, what is the cause?

Labels (1)
0 Kudos
Reply
0 Replies