Problem with LCD peripherals ( No LCD_ENAB_M) [ SOLVED ]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with LCD peripherals ( No LCD_ENAB_M) [ SOLVED ]

974件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leform14 on Tue Jan 13 06:07:11 MST 2015
Hello,

I try to use a TFT-panel with a lpc1788. I use as reference the source code for MOD-LCD.4.3"+ evaluation board. My config are good, I see my DOTCLK at the good speed but I can't see anything on the pin 2.4 (LCD_Enable_m). The mux register is set to FUNC_7, TFT and other parameters are ok but nothing appears on my screen except ugly bar of any color. I set a buffer of y lines and x pixels that I used as UpperPanel Frame base (single mode) but nothing ...
Anybody can help me to do a check of what I have done or give me tips please ?
ラベル(1)
0 件の賞賛
返信
1 返信

966件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leform14 on Wed Jan 14 03:44:36 MST 2015
HI all,

I solved my problem, that was due to the buffer (I use now 0x20000000). So now, I am able to use the mod-LCD.4.3"+ board with a code based on FreeRTOS/lpcOpen library (draw/cursor) and external SDRAM (buffer is now Dynamic memory chip select X address).

Thanks
0 件の賞賛
返信