Problem with Flash Magic Bootlader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with Flash Magic Bootlader

1,716 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by milind.mishra on Thu Apr 16 23:22:34 MST 2015
Hi,

I have modified a sample bootloader code provided by flash magic to support firmware flashing using SPIFI interface.
I changed the code from supporting LPC18xx to supporting LPC43xx. I am using Keil uv4 for doing that.

Most of the files are getting compiled but towards the end the Linker throws an error which I am unable to comprehend.

Kindly look at the screenshot and provide some possible leads to fix this problem.

Regards,
Milind.
Labels (1)
0 Kudos
Reply
0 Replies