Problem on LPC2148 I2C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem on LPC2148 I2C

2,253件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rajavarmanslr on Mon Jun 13 05:22:40 MST 2016
[h2]  **-------------------------------------------CODE 1-----------------------------------------** [/h2]

    #include<lpc214x.h>
    
    void ser_init(void);
    void tx(unsigned char c);
    unsigned char rx(void);
    void tx_string(unsigned char *s);
    
    void i2c_init(void);
    void write(unsigned char data,unsigned char addr);
    unsigned char read(unsigned char addr);
    
    int main()
    {
    unsigned char temp;
    ser_init();
    i2c_init();
    tx_string("Writing\n\r");
    write('A',0x00);
    tx_string("Write successfully...\n\r");
    tx_string("Reading...\n\r");
    temp=read(0x00);
    tx_string("Received data is : ");
    tx(temp);
    while(1);
    }
    
    void i2c_init()
    {
    PINSEL0|=0x50;
    I2C0SCLH=75;
    I2C0SCLL=75;
    }
    
    void write(unsigned char data,unsigned char addr)
    {
    unsigned char addL,addH;
    
    addL=addr&0xff;
    addH=(addr&0xff) >>8;
    
    I2C0CONCLR=0x000000FF; //Clear all I2C settings
    I2C0CONSET=1<<6;//I2EN=1
    I2C0CONSET=1<<5;//Start
    while(I2C0STAT != 0x08);
    I2C0CONCLR=(1<<5)|(1<<3);//Clear Start and Interrupt
    
    I2C0DAT = 0xA0;
    I2C0CONSET=1<<2;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x18);
    
    I2C0DAT = addH;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x28);
    I2C0DAT = addL;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x28);  
    
    I2C0DAT = data;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x28);
    I2C0CONCLR=(1<<3);//Clear Interrupt
    I2C0CONSET=1<<4;//Stop
    }
    
    unsigned char read(unsigned char addr)
    {
    unsigned char read=0,addL,addH;
    addL=addr&0xff;
    addH=(addr&0xff00)>>8;
    
    I2C0CONCLR=0x000000FF; //Clear all I2C settings
    I2C0CONSET=1<<6;//I2EN=1
    I2C0CONSET=1<<5;//Start
    while(I2C0STAT != 0x08);
    I2C0CONCLR=(1<<5)|(1<<3);//Clear Start and Interrupt
    
    I2C0ADR = 0xA0;
    I2C0DAT = 0xA0;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x18);
    
    I2C0DAT = addH;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x28);
    I2C0DAT = addL;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x28);
    
    I2C0CONSET=(1<<2)|(1<<5); //Start
    I2C0CONCLR=(1<<3);//Clear Interrupt
    while(I2C0STAT != 0x10);
    
    I2C0ADR = 0xA1;
    I2C0DAT = 0xA1;
    I2C0CONCLR=(1<<3) | (1<<5);//Clear Interrupt , Start
    while(I2C0STAT != 0x40);
    I2C0CONCLR=(1<<3);//Clear Interrupt
    
    while(I2C0STAT != 0x50);
    read=I2C0DAT;
    I2C0CONCLR=(1<<3);//Clear Interrupt
    
    I2C0CONCLR=(1<<3);//Clear Interrupt
    I2C0CONSET=1<<4;
    
    return read;
    }
    
    void ser_init()
    {
    VPBDIV=0x02;
    PINSEL0|=0x05;
    U0LCR=0x83;
    U0DLL=195;
    U0DLM=0;
    U0LCR=0x03;
    U0TER=(1<<7);
    
    }
    
    void tx(unsigned char c)
    {
    U0THR=c;
    while((U0LSR&(1<<5))==0);
    }
    
    void tx_string(unsigned char *s)
    {
    while(*s)
    {
    tx(*s++);
    }
    }
    
    unsigned char rx()
    {
    while((U0LSR&(1<<0))==0);
    return U0RBR;
    }


[h2]**--------------------------------------CODE 2-----------------------------------------**[/h2]

   
#include<lpc214x.h>
    
    #define delay for(i=0;i<100000;i++)
    #define FALSE 0
    #define TRUE 1
    unsigned long int i;
    
    void i2c_init(void);
    unsigned char check_status(unsigned char status);
    unsigned char i2c_write(unsigned char data,unsigned char status);
    unsigned char i2c_read(void);
    unsigned char send_byte(unsigned char data,unsigned char address);
    unsigned char read_byte(unsigned char address);
    void i2c_delay(void);
    
    void ser_init(void);
    void tx(unsigned char c);
    unsigned char rx(void);
    void tx_string(unsigned char *s);
    
    int main(void)
    {
    ser_init();
    tx_string("I2C INTERFACING\n\r");
    send_byte('w',0x00);
    delay;
    tx_string("I2C Write\n\r");
    delay;
    tx(read_byte(0x01));
    while(1);
    }
    
    void ser_init()
    {
    VPBDIV=0x02;
    PINSEL0|=0x05;
    U0LCR=0x83;
    U0DLL=195;
    U0DLM=0;
    U0LCR=0x03;
    U0TER=(1<<7);
    
    }
    
    void tx(unsigned char c)
    {
    U0THR=c;
    while((U0LSR&(1<<5))==0);
    }
    
    void tx_string(unsigned char *s)
    {
    while(*s)
    {
    tx(*s++);
    }
    }
    
    unsigned char rx()
    {
    while((U0LSR&(1<<0))==0);
    return U0RBR;
    }
    
    void i2c_init(void)
    {
    PCONP|= 0x00000080;// Power on I2C0 peripheral
    PINSEL0 |= 0x50;/*Initialize Pin Connect Block P0.2 as SCL0 P0.3 as SDA0*/
    I2C0CONCLR = 0x6C;/*Clear AA, I2C Interrupt Flag, Start Bit*/
    I2C0CONSET = 0x40;/*Enable I2C0*/
    /*I2C0SCLH = 75;
    I2C0SCLL = 75;*/
    I2C0SCLH = 14745600/(2*50000);
    I2C0SCLL = 14745600/(2*50000);
    }
    
    
    
    unsigned char check_status(unsigned char status)
    {
    unsigned long int time=0;
    while(time<300000)
    {
    if(I2C0CONSET & 1<<3)
    {
    if (I2C0STAT == status)
    {
    return TRUE;
    }
    }
    time++;
    }
    return FALSE;
    }
    
    unsigned char i2c_write(unsigned char data,unsigned char status)
    {
    I2C0DAT = data & 0xFF;;
    I2C0CONCLR = 0X2C;
    if(!check_status(0x08))/*Wait for the Status Set*/
    return FALSE;
    else
    return TRUE;
    }
    
    unsigned char i2c_read(void)
    {
    I2C0CONCLR= 0x2C;// clear all except I2EN 
    if(!check_status(0x58))/* Wait for Status Set - 0x58 */
    return FALSE;
    i2c_delay();
    return (char)I2C0DAT;
    }
    
    unsigned char send_byte(unsigned char data,unsigned char address)
    {
    //-------------------START--------------------------------------------
    
    I2C0CONSET = 0x20;/*Set the Start Bit*/
    if(!check_status(0x08))/*Wait for the Status Set*/
    return FALSE;
    
    //------------------SEND SLAVE ADDRESS---------------------------------
    
       i2c_delay();
    if(!i2c_write(0xA0,0x18))
    return FALSE;
    
    //------------------SEND ADDRESS--------------------------------------
    
    i2c_delay();
    if(!i2c_write(address,0x28))
    return FALSE;
    
    //------------------SEND DATA----------------------------------------
    
    i2c_delay();
    if(!i2c_write(data,0x28))
    return FALSE;
    
    //-------------------STOP---------------------------------------------
    
    i2c_delay();
    I2C0CONSET= 0x10;// generate stop condition
    I2C0CONCLR= 0x2C;
    
    return TRUE;
    }
    
    unsigned char read_byte(unsigned char address)
    {
    unsigned char read;
    i2c_init();
    //-------------------START--------------------------------------------
    
    I2C0CONSET = 0x20;/*Set the Start Bit*/
    if(!check_status(0x08))/*Wait for the Status Set*/
    return FALSE;
    
    //------------------SEND SLAVE ADDRESS---------------------------------
    
       i2c_delay();
    if(!i2c_write(0xA0,0x18))
    return FALSE;
    
    //------------------SEND ADDRESS--------------------------------------
    
    i2c_delay();
    if(!i2c_write(address,0x28))
    return FALSE;
    
    I2C0CONCLR= 0x08;// clear SI flag
    I2C0CONSET= 0x10;// generate stop condition
    
    //-------------------START--------------------------------------------
    
    I2C0CONSET = 0x20;/*Set the Start Bit*/
    if(!check_status(0x08))/*Wait for the Status Set*/
    return FALSE;
    
    //------------------SEND READ ADDRESS--------------------------------------
    
    I2C0DAT = 0xA1;
    I2C0CONCLR= 0x28;// clear all except I2EN and AA
    if(!check_status(0x40))/*Wait for the Status Set*/
    return FALSE;
    
    //----------------------READ-------------------------------------------------
    
    read = i2c_read();
    //-------------------STOP---------------------------------------------
    
    i2c_delay();
    I2C0CONSET= 0x10;// generate stop condition
    I2C0CONCLR= 0x2C;
    
    return read;
    }
    
    
    void i2c_delay()
    {
    unsigned long int i2c_del;
    for(i2c_del=0;i2c_del<=100000;i2c_del++);
    }


This is my I2C code with LPC2148. But these codes are not working. Please help me in this problem. Thanks in advance

Original Attachment has been moved to: code%201.rar

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,891件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,891件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Mon Jun 13 06:43:17 MST 2016
What is "not working". What are you expecting to happen, and what is actually happening. Without more information we cannot help!
0 件の賞賛
返信