LPC11U24 Active Mode Supply Current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U24 Active Mode Supply Current

1,162 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by karl__34 on Mon Jun 13 16:42:01 MST 2016
I am currently working with the LPC11U24 on the NTAG I2C Plus board and finding that even with the following configuration in the demo code:

Chip_SYSCTL_PowerUp(SYSCTL_POWERDOWN_WDTOSC_PD);
LPC_SYSCTL->SYSAHBCLKCTRL |= (1<<15);  // enable clock to WDT block
Chip_Clock_SetWDTOSC(WDTLFO_OSC_4_60, 2);
LPC_WWDT->CLKSEL |= (1<<0);  // select watchdog oscillator
Chip_Clock_SetMainClockSource(SYSCTL_MAINCLKSRC_WDTOSC);

That the board (without LCD attached) is consuming ~1.4-1.6mA.

Is there an active mode configuration for this board and microcontroller that can result in something in the region of 0.5mA?

Thanks,
Karl

Labels (1)
0 Kudos
Reply
1 Reply

1,121 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply