Problem caused by a difference between two demo board revision ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem caused by a difference between two demo board revision ?

ソリューションへジャンプ
3,476件の閲覧回数
benjamin3
Contributor I

Hello,


I have a problem with the code example from a SDK from NXP about the EMC bus to use an external SDRAM. I use the LPCXpresso 546xx/540xx demo board from NXP.

The code example works correctly when I use the demo board LPCxpresso546xx/540xx with an external SDRAM from Micron ( MT48LC8M16A2B4) but when I use the demo board LPCxpresso546xx/540xx with an external SDRAM from Winbond (W9812G6JB-6I), the program says that there is an error when it checks the written data in the external SDRAM memory.

I was able to see in the memory that there is an error during data writing step :

Normally, the program writes (from the 0xA0000000 address) data from 0 and increasing each value by 1 compared with the previous value (ex : 00000000, 00000001, ...., 0000000A, 0000000B). However, at an address the written value is not correct compared with the others (ex : 000002FC, 000002FD, 000002FE, 6B836021, 00000300, 00000301, the wrong value is at the address 0xa0000bfc but at each try, the address with the wrong value is not the same).

Best regards,

Benjamin

ラベル(1)
0 件の賞賛
返信
1 解決策
3,316件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Benjamin Hainaut,

Thanks for your reply.
I only have one rev E board on hand, it's LPCXpresso54018.

pastedImage_1.jpg
It doesn't encounter a similar error as you mentioned above when running the emc_sdram code.

pastedImage_2.png
I've also attached the BOARD_InitSDRAM() function below, please check it.

#ifdef W9812G6JB6I
#define SDRAM_REFRESHPERIOD_NS (64 * 1000000 / 4096) /* 4096 rows/ 64ms */
#define SDRAM_TRP_NS (20u)
#define SDRAM_TRAS_NS (42u)
#define SDRAM_TSREX_NS (72u)
#define SDRAM_TAPR_NS (18u)
#define SDRAM_TWRDELT_NS (12u)
#define SDRAM_TRC_NS (60u)
#define SDRAM_RFC_NS (60u)
#define SDRAM_XSR_NS (67u)
#define SDRAM_RRD_NS (12u)
#define SDRAM_MRD_NCLK (2u)
#define SDRAM_RAS_NCLK (2u)
#define SDRAM_MODEREG_VALUE (0x23u)
#define SDRAM_DEV_MEMORYMAP (0x09u) /* 128Mbits (8M*16, 4banks, 12 rows, 9 columns)*/
#endif

/* Initialize the external memory. */
void BOARD_InitSDRAM(void)
{
    emc_basic_config_t basicConfig;
    emc_dynamic_timing_config_t dynTiming;
    emc_dynamic_chip_config_t dynChipConfig;

    /* Basic configuration. */
    basicConfig.endian = kEMC_LittleEndian;
    basicConfig.fbClkSrc = kEMC_IntloopbackEmcclk;
    /* EMC Clock = CPU FREQ/2 here can fit CPU freq from 12M ~ 180M.
     * If you change the divide to 0 and EMC clock is larger than 100M
     * please take refer to emc.dox to adjust EMC clock delay.
     */
    basicConfig.emcClkDiv = 1;
    /* Dynamic memory timing configuration. */
    dynTiming.readConfig = kEMC_Cmddelay;
    dynTiming.refreshPeriod_Nanosec = SDRAM_REFRESHPERIOD_NS;
    dynTiming.tRp_Ns = SDRAM_TRP_NS;
    dynTiming.tRas_Ns = SDRAM_TRAS_NS;
    dynTiming.tSrex_Ns = SDRAM_TSREX_NS;
    dynTiming.tApr_Ns = SDRAM_TAPR_NS;
    dynTiming.tWr_Ns = (1000000000 / CLOCK_GetFreq(kCLOCK_EMC) + SDRAM_TWRDELT_NS); /* one clk + 6ns */
    dynTiming.tDal_Ns = dynTiming.tWr_Ns + dynTiming.tRp_Ns;
    dynTiming.tRc_Ns = SDRAM_TRC_NS;
    dynTiming.tRfc_Ns = SDRAM_RFC_NS;
    dynTiming.tXsr_Ns = SDRAM_XSR_NS;
    dynTiming.tRrd_Ns = SDRAM_RRD_NS;
    dynTiming.tMrd_Nclk = SDRAM_MRD_NCLK;
    /* Dynamic memory chip specific configuration: Chip 0 - W9812G6JB-6I */
    dynChipConfig.chipIndex = 0;
    dynChipConfig.dynamicDevice = kEMC_Sdram;
    dynChipConfig.rAS_Nclk = SDRAM_RAS_NCLK;
    dynChipConfig.sdramModeReg = SDRAM_MODEREG_VALUE;
    dynChipConfig.sdramExtModeReg = 0; /* it has no use for normal sdram */
    dynChipConfig.devAddrMap = SDRAM_DEV_MEMORYMAP;
    /* EMC Basic configuration. */
    EMC_Init(EMC, &basicConfig);
    /* EMC Dynamc memory configuration. */
    EMC_DynamicMemInit(EMC, &dynTiming, &dynChipConfig, 1);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
3,316件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Benjamin Hainaut ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Before answering the question, I was wondering if you can introduce the condition and steps of replicating the phenomenon, for instance, the demo boards, demo code, etc, as it will help me to figure it out.
Looking forward to your reply.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,316件の閲覧回数
benjamin3
Contributor I

I use a LPCXpresso546xx/540xx revision E and for the test, I use the emc_sdram program from SDK_2.5.0_LPCXpresso54628.
Yesterday, I modified the specific time "SDRAM_TRP_NS" in the file "board.c" with the other specific times with the values given in the datasheet from Winbond. The error is again present but when I modify the SDRAM_TRP_NS value with higher value than value in datasheet, there is not error left.
Other interesting fact : when I set the frequency of the EMC bus to 110 MHz (after setting the AHB bus' clock to 220 MHz), the value given in datasheet (for SDRAM_TRP_NS) doesn't cause error anymore.

0 件の賞賛
返信
3,317件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Benjamin Hainaut,

Thanks for your reply.
I only have one rev E board on hand, it's LPCXpresso54018.

pastedImage_1.jpg
It doesn't encounter a similar error as you mentioned above when running the emc_sdram code.

pastedImage_2.png
I've also attached the BOARD_InitSDRAM() function below, please check it.

#ifdef W9812G6JB6I
#define SDRAM_REFRESHPERIOD_NS (64 * 1000000 / 4096) /* 4096 rows/ 64ms */
#define SDRAM_TRP_NS (20u)
#define SDRAM_TRAS_NS (42u)
#define SDRAM_TSREX_NS (72u)
#define SDRAM_TAPR_NS (18u)
#define SDRAM_TWRDELT_NS (12u)
#define SDRAM_TRC_NS (60u)
#define SDRAM_RFC_NS (60u)
#define SDRAM_XSR_NS (67u)
#define SDRAM_RRD_NS (12u)
#define SDRAM_MRD_NCLK (2u)
#define SDRAM_RAS_NCLK (2u)
#define SDRAM_MODEREG_VALUE (0x23u)
#define SDRAM_DEV_MEMORYMAP (0x09u) /* 128Mbits (8M*16, 4banks, 12 rows, 9 columns)*/
#endif

/* Initialize the external memory. */
void BOARD_InitSDRAM(void)
{
    emc_basic_config_t basicConfig;
    emc_dynamic_timing_config_t dynTiming;
    emc_dynamic_chip_config_t dynChipConfig;

    /* Basic configuration. */
    basicConfig.endian = kEMC_LittleEndian;
    basicConfig.fbClkSrc = kEMC_IntloopbackEmcclk;
    /* EMC Clock = CPU FREQ/2 here can fit CPU freq from 12M ~ 180M.
     * If you change the divide to 0 and EMC clock is larger than 100M
     * please take refer to emc.dox to adjust EMC clock delay.
     */
    basicConfig.emcClkDiv = 1;
    /* Dynamic memory timing configuration. */
    dynTiming.readConfig = kEMC_Cmddelay;
    dynTiming.refreshPeriod_Nanosec = SDRAM_REFRESHPERIOD_NS;
    dynTiming.tRp_Ns = SDRAM_TRP_NS;
    dynTiming.tRas_Ns = SDRAM_TRAS_NS;
    dynTiming.tSrex_Ns = SDRAM_TSREX_NS;
    dynTiming.tApr_Ns = SDRAM_TAPR_NS;
    dynTiming.tWr_Ns = (1000000000 / CLOCK_GetFreq(kCLOCK_EMC) + SDRAM_TWRDELT_NS); /* one clk + 6ns */
    dynTiming.tDal_Ns = dynTiming.tWr_Ns + dynTiming.tRp_Ns;
    dynTiming.tRc_Ns = SDRAM_TRC_NS;
    dynTiming.tRfc_Ns = SDRAM_RFC_NS;
    dynTiming.tXsr_Ns = SDRAM_XSR_NS;
    dynTiming.tRrd_Ns = SDRAM_RRD_NS;
    dynTiming.tMrd_Nclk = SDRAM_MRD_NCLK;
    /* Dynamic memory chip specific configuration: Chip 0 - W9812G6JB-6I */
    dynChipConfig.chipIndex = 0;
    dynChipConfig.dynamicDevice = kEMC_Sdram;
    dynChipConfig.rAS_Nclk = SDRAM_RAS_NCLK;
    dynChipConfig.sdramModeReg = SDRAM_MODEREG_VALUE;
    dynChipConfig.sdramExtModeReg = 0; /* it has no use for normal sdram */
    dynChipConfig.devAddrMap = SDRAM_DEV_MEMORYMAP;
    /* EMC Basic configuration. */
    EMC_Init(EMC, &basicConfig);
    /* EMC Dynamc memory configuration. */
    EMC_DynamicMemInit(EMC, &dynTiming, &dynChipConfig, 1);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,316件の閲覧回数
benjamin3
Contributor I

Hi,

Thank you for your answer, it works correctly.

The problem went from a wrong setting of the specific times (SDRAM_TRP_NS, SDRAM_TRAS_NS ect ...).

Have a nice day,

Benjamin

0 件の賞賛
返信