Problem UART Interrupt LPC2134

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem UART Interrupt LPC2134

2,293 Views
robertorober
Contributor I

First hello to everyone.

Sorry for my English.

I tell you.

I'm starting to use microcontrollers ARM7 specifically the LPC2134 and I am performing a bidirectional serial communication.

The program consists blink an LED to verify that the system is working, and UART communication with a PC and a serial adapter to convert levels.

My purpose is to use a vectored IRQ interrupt, so that when some data arrives the program stops and observe the interrupt and save the received data in an array for later processing.

In addition I make a bluque sending the ASCII table to the PC.

My problem is that encuanto recivo a data interruption jumps and I can not in any way out of it by staying in an infinite loop in the interruption.

The program I'm doing with the KEIL 4.

 

Main Program

int main()

    {

    Init_pll();

    VICIntEnClr=0xFFFF;//Borro cualquier posible interrupcion

    Init_gpio();

    init_uart();

    i=0;                                  

    while (1)

       {

       for(i=0;i<256;i++)

          {

           LED_blink ();//Parpadeo del LED

     ENVIA_BYTETX0(i);

     }                                                   

      }   

   }

 

UART CONFIGURATION

void init_uart(void)

    {      

    U0LCR=0x03;

    U0FDR=0x10;//Multivall a 1

    U0LCR|=BIT7;//Activo Bit DLAB para poder configurar velocidad        

    U0DLL=divisor & 0xFF;

    U0DLM = (divisor >> 8) & 0xFF;

    U0LCR &=~BIT7;//Borro Bit DLAB para poder configurar velocidad        

    U0FCR=1;//Activo FIFO        

    U0IER = 0;//Desabilito interrupciones UART 1

       

    VICIntSelect &= ~(1<<UART_0);

    VICDefVectAddr |= (1<<UART_0);

    VICVectCntl10 = 0x20 | UART_0;                     /* Prioridad 0 Vectorizada use it for UART 0 Interrupt*/

    VICVectAddr10 = (unsigned long)RX_UART_CERO ;           /* set interrupt vector in 0   */

    VICIntEnable |= BIT6;                   /* Enable UART0 Interrupt     */

    U0IER = 1;//Habilito interrupcion de recepcion de datos validos

    }

 

INTERRUPT

_irq void RX_UART_CERO (void)

   {

   if(U0IIR&DR)      // Infinite loop

      {        

      while (!(U0LSR&DR));

      if(PUNT_W0<512)

         {

         BUFFER_UART0[PUNT_W0]=U0RBR;

         PUNT_W0++;

         }

      else;

      }

   else;

   VICVectAddr &= 0x0000;//Clear Flag Interrupts but not exit and return to Infinite loop                               

   }

 

Everything works fine until you receive date UART in the LPC. Then jumps to the interruption and there does not come out.

No longer what to do, I take several days reading the datasheet and reviewing the program, but can not find anything wrong.

I request help from someone who can guide me to solve the problem and continue learning.

 

Thanks you very much.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,979 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Roberto,

It seems that your code is not clearing the U0IIR register, which indicates if there is a pending interrupt, causing a loop on the ISR. For further details, you could refer to the following links:

http://www.keil.com/forum/20979/

http://www.nxp.com/documents/application_note/AN10414.pdf

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,979 Views
robertorober
Contributor I

Ok.

Thanks you very much Carlos.

Thanks to your help I could solve the problem.

Best regards.

Roberto

0 Kudos
Reply