Primary CAN bootloader LPC11C24, Problem to start user app (CAN ISP Go G)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Primary CAN bootloader LPC11C24, Problem to start user app (CAN ISP Go G)

1,475件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lea on Sat Feb 13 02:29:55 MST 2016
When I flash new firmware under use of the primary CANopen bootloader I send over CAN

1. SDO Execution Address (Index: 0x5070) and after that
2. SDO Program Control (Index: 0x1F51, value = 0x01)

When the primary bootloader is running the start of the new firmware only is done when I set PI0_1 = low before call
But this is not really what I want. In most cases it is not possible to change the state of this pin, when the device is installed.

Is there a way to do this without change the status of PI0_1?

Supplement: After a reinvoke to start the primary bootloader from user app again, it' not possible to start the firmware with step 1 and 2.
Only a hardware reset let start the new firmware.
ラベル(1)
0 件の賞賛
返信
1 返信

1,347件の閲覧回数
p0ulp3
Contributor I

Hello,

 

I am facing a similar issue, no way to start the app except by hw reset. Did you find any way to solve this out ?


Regards

0 件の賞賛
返信