Presentation material on the LPC80x Switch Matrix

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Presentation material on the LPC80x Switch Matrix

ソリューションへジャンプ
2,939件の閲覧回数
drsmith_yorku
Contributor III

Hi,

I'm looking for the PPTX slides for the presentation on the LPC80x Switch Matrix that are featured in the video on the NXP webpage (LPC80x微控制器系&#210|NXP ).  Some of the images are really hard to view because they are in low resolution.

thanks!

James

ラベル(2)
0 件の賞賛
返信
1 解決策
2,815件の閲覧回数
soledad
NXP Employee
NXP Employee

Please check the attachment. 

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,815件の閲覧回数
drsmith_yorku
Contributor III

Thanks!  That's perfect.

all the best,

James

0 件の賞賛
返信
2,816件の閲覧回数
soledad
NXP Employee
NXP Employee

Please check the attachment. 

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信