I need 3 PWM signals to control 3 servos.
I need a rate with 50Hz = 20ms.
The duty cycle should be from about 0,9 ms to 2 ms.
LPC_SC->PCONP |= 1 << 6; // Set PWM1 power7clock control bit
LPC_SC->PCLKSEL0 |= 1 << 12; // Peripheral clock selection for Timer2 ; PWM clock = microcontroller clock i.e the prescaler value is 1.
LPC_PINCON->PINSEL4 = (0x1<<0) | (0x1<<2) | (0x1<<4); // Set Output P2.0 P2.1 P2.2 as PWM1.1 PWM1.2 PWM1.3
LPC_PINCON->PINMODE4 |= 1 << 9; // enable neither pull up nor pull down.
LPC_PWM1->MR0 = 20000; // PWM freq = 50 Hz = 20 ms
LPC_PWM1->MCR |= 1 << 1; // Reset timer on Match0
LPC_PWM1->MR5 = 1000; // PWM Duty Cycle = 1000 Hz = 1 ms
LPC_PWM2->MR3 = 1500; // PWM Duty Cycle = 1000 Hz = 1 ms LPC_PWM3->MR4 = 2000; // PWM Duty Cycle = 1000 Hz = 1 ms
LPC_PWM1->TCR |= (1 << 0) | (1 << 3);
I use the LPC1769
The settings are right? Will I get 3 different PWM signals at the output pins?
SERVO Motor with PWM Signal