PWM configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PWM configuration

3,091 次查看
ranjithshanbhag
Contributor III

Kerry Zhou

In attached sample code can you help me how to configure PWM in center aligned mode?

 

Path: LPC824_Example_Code_Bundle_IAR_r1.0\Example_SCT_PWM_2State\src

Original Attachment has been moved to: LPC824_Example_Code_Bundle_LPCXpresso_r1.0.zip

0 项奖励
回复
7 回复数

2,759 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ranjith Shanbhag,

    Thank you for your trust.

    Do you just want to configure the counter to up-down mode?

    If yes, please modify the  SCT control register, BIDIR_L and BIDIR_H to 1.

  Just like the user manual, SCT regiser description:

pastedImage_1.png

Please try it on your side.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,759 次查看
ranjithshanbhag
Contributor III

Hi kerryzhou‌,

Thank you for your valuable reply.

What all configuration changes required? By modifying SCT control register, BIDIR_L and BIDIR_H to 1 i am unable to aceive it.
Please help me.

Regards,

Ranjith Shanbhag

0 项奖励
回复

2,759 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ranjith Shanbhag,

   I don't know why you said configure BIDIR_L and BIDIR_H to 1 unable to work?

  I just modify these two bits, it works on my side.

  As you know, CPWM will make the counter to up-down, so the frequency will half of the original counter up.

  This is my test result and code is in the attachment.
This project will generate 250hz at PIO0_16, 50khz PWM at PIO0_12.

pastedImage_1.png

pastedImage_2.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,759 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ranjith Shanbhag,

  How did you know it  can't achieve it?

  Please give me your test result, and tell me the details how your analysis it. I will check it.

 If it is really not OK, I will test it on my side when I have time.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,759 次查看
ranjithshanbhag
Contributor III

Hi kerryzhou‌,

With reference to AN11538 SCTimer/PWM cookbook (page no 15) i have done modification in the code and tested. i am unable to get PWM output.

i need your help to move forward in my project. Please provide your thoughts.

Please find the below link for the project which you shared earlier and in same project i need center aligned configuration.
https://community.nxp.com/message/869082?commentID=869082&et=watches.email.thread#comment-869082 

Path: LPC824_Example_Code_Bundle_IAR_r1.0\Shared_Project_Source_Code\Example_SCT_PWM_2State\src

0 项奖励
回复

2,759 次查看
ranjithshanbhag
Contributor III

hi kerryzhou,

Any update on above discussion?

Regards,

Ranjith

0 项奖励
回复

2,759 次查看
ranjithshanbhag
Contributor III

Sorry @Kerry Zhou i attached wrong project. Please find the below link for the project
https://community.nxp.com/message/869082?commentID=869082&et=watches.email.thread#comment-869082 

Path: LPC824_Example_Code_Bundle_IAR_r1.0\Shared_Project_Source_Code\Example_SCT_PWM_2State\src

0 项奖励
回复