PCF2129 RTC with OM13092

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF2129 RTC with OM13092

ソリューションへジャンプ
2,130件の閲覧回数
fatihozen
Contributor IV

Hello,

I have PCF2129T and OM13092 Dev. Board ( LPC54608 ).  I wanna have updated time in my projects and testing this RTC. I chose I2C for communication and added a battery to RTC. But when I cut the power from board and then repower it, RTC datas gone away. It shows strange datas. I changed battery once and still same result. Project in attachment. It seems battery is not working. Battery voltage is 2,941 V now. Any suggestion ?

no battery:
pastedImage_2.png

with battery(similar result):
pastedImage_3.png


connection is like :

pastedImage_4.png

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,957件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fatih,

I suppose that the second/minute/hour/month/year registers lose their value after you power off both the power supply from VDD pin and battery power supply  from Vbat pin, you have to write the initial value to the second/minute/hour/month/year registers after you power on again.

This is LPC micro controller forum, for PCF2129 question, it appear you can post a ticket to the link:

https://community.nxp.com/community/other 

Hope it can help you

BR

Xiangjun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,958件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fatih,

I suppose that the second/minute/hour/month/year registers lose their value after you power off both the power supply from VDD pin and battery power supply  from Vbat pin, you have to write the initial value to the second/minute/hour/month/year registers after you power on again.

This is LPC micro controller forum, for PCF2129 question, it appear you can post a ticket to the link:

https://community.nxp.com/community/other 

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信
1,957件の閲覧回数
fatihozen
Contributor IV

Thank you, this solved my problem.

0 件の賞賛
返信