Output Gate Driver MC33908 with LPC54102 via SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output Gate Driver MC33908 with LPC54102 via SPI

1,764 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Tue Dec 29 22:25:00 MST 2015
Hello,

I have connected via SPI LPC54102 to the MC33908. The MC33908 has two pins IO_4 and IO_5 that can be used as output driver gate.


Quote:
Output gate driver: Can drive a logic level low-side NMOS transistor. Controlled by the SPI.



I am not clear how to connect to a Dual NMOS (BUK7K5R1-30E).

Is mandatory to connect a 5.1K resistor in serie?

I have made an example (attached) but I guess that is not work.


Best Regards.
Labels (1)
0 Kudos
Reply
0 Replies