Om13085 code not executing/starting after Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Om13085 code not executing/starting after Reset

1,290件の閲覧回数
ronwal
Contributor III

I´m using the the OM13085 and somehow the code is only executing when connected to the IDE/debugger and right after the firmware have been flashed.

If I reset the board or switch it off and on the code is not executing...

My project is based on the uIP/webserver samples.

Any idea?

Thanks

br Ron

ラベル(1)
0 件の賞賛
返信
1 返信

1,208件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Hi Ron,

I think you also posted this question as response to a previous thread:

https://community.nxp.com/thread/435247?sr=stream

Since I answered that one, I am marking this thread as assumed answered too.

Regards,

Brendon

0 件の賞賛
返信